VM.STOP

Description

VM.STOP stops execution of the program. Use VM.START to start program execution at the point in the program VM.STOP was commanded.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1160

No Command No

M_01-05-11-000

Related Topics

VM.START